Skip to main content
Associate II
Aug 23, 2023 7:51 AM UTC
Solved

Is it possible to zoom in using two fingers in Touch GFX Designer?

Hi, I have a question about the touch operation in the TouchGFX Designer.
I want to enlarge the display by spreading two fingers like a smartphone browser, but I can't find it even if I check the demo screen.
If it is possible to operate with two fingers, please point me to a page showing a usage example.

    This topic has been closed for replies.
    Osman SOYKURT
    Osman SOYKURTBest answer
    ST Technical Moderator
    Aug 23, 2023 11:23 AM UTC

    Hello @TN_it ,

    TouchGFX doesn't support multi touch. The TouchController interface is based on a single set of coordinates and whether a touch was registered or not.

     /**
     * Samples the position of the mouse cursor.
     *
     * @param [out] x The x coordinate.
     * @param [out] y The y coordinate.
     *
     * @return True if touch detected, false otherwise.
     */
     bool doSampleTouch(int32_t& x, int32_t& y) const;
    ST Software Developer | TouchGFX

    2 replies

    Osman SOYKURT
    Osman SOYKURTBest answer
    ST Technical Moderator
    Aug 23, 2023 11:23 AM UTC

    Hello @TN_it ,

    TouchGFX doesn't support multi touch. The TouchController interface is based on a single set of coordinates and whether a touch was registered or not.

     /**
     * Samples the position of the mouse cursor.
     *
     * @param [out] x The x coordinate.
     * @param [out] y The y coordinate.
     *
     * @return True if touch detected, false otherwise.
     */
     bool doSampleTouch(int32_t& x, int32_t& y) const;
    ST Software Developer | TouchGFX
    TN_itAuthor
    Associate II
    Aug 24, 2023 4:38 AM UTC

    Thank you for answering, @Osman SOYKURT .

    I understand that it is not possible to distinguish between multiple coordinates.

    I will consider zooming in using other touch operations.