Skip to main content
MSale.1
Senior
Apr 1, 2020 7:35 AM UTC
Question

Is it possible to convert with DMA2D on STM32H743 YCBCR from the DCMI to RGB565 ?

I have question related to the graphic engine DMA2D in the STM32H743. Can it convert progressive scan YCBCR from the DCMI to RGB 565. this is very important for any Application that needs to save video at high resolution with 30fps?

This topic has been closed for replies.

7 replies

berendi
Principal
Apr 1, 2020 8:11 AM UTC

The incoming YCbCr data format is documented in section 18.4.12 YCbCr support of the reference manual. If the ordering is different, you have to rearrange it beforehand by a separate pass, maybe through DMA2D or MDMA.

MSale.1
MSale.1Author
Senior
Apr 1, 2020 8:26 AM UTC

@berendi​  I read it before but it also mention that it work with the output of the hardware JPEG decoder which is 8x8 block. so is it ok to use the same configuration with the output from the camera?

Thanks in advance

ST Technical Moderator
Apr 1, 2020 8:25 AM UTC

Hello,

I recommend you this AN5020: Digital Camera Interface (DCMI) on STM32 MCUs that will help you in your configuration.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MSale.1
MSale.1Author
Senior
Apr 1, 2020 8:29 AM UTC

@Imen DAHMEN​ 

Hello,

Thanks for the answer.i just have asked specific question because i could not found any information about it and with software conversion it will take time which will affect the frame rate. i hope i got direct answer from you to my question.

Regards

Mahmoud

ST Technical Moderator
Apr 1, 2020 10:43 AM UTC

Yes, it is possible to convert with DMA2D on STM32H743 YCbCr to RGB565

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks