Skip to main content
GS1
Senior III
May 23, 2023 12:39 PM UTC
Question

Is it possible to adapt the time factor for the automatically created number of ticks for fade times?

When defining a fade duration of e.g. 350 msTouchGFX generates a tick time of 21 ticks based on the 60 Hz LCD update rate.

My LCD now had to be adapted to only have an update rate of appx. 30 Hz. Then the fade duration is double in time.

Is there a way to define the number of ticks which TouchGFX uses per 100 ms or maybe the LCD update rate, so the used number of ticks fits to the wanted time?

Thanks for any proposals.

BR GS

This topic has been closed for replies.