Skip to main content
Charles P
Associate II
December 6, 2021
Question

Is it okay for TouchGFX function model::tick() to share resources with ThreadX, even though ThreadX is not aware of model::ticks() existence? Can they use the same mutex?

In my configuration, the tick source for touchGFX is the LTDC vsync interrupt. This was the recommended configuration in STM32CubeMX. However, that means that ThreadX is doing its own thing while model::tick (e.g., TouchGFX) is also running. The ThreadX timer priority is 0, whereas the LTDC priority is 10. Are there potential pitfalls to having a message queue or mutex to share a common resource between the two?

The documentation here seems to indicate that what I have described above is the prescribed method. I just want to make sure there are no issues with the two threads being unaware of ech other. https://support.touchgfx.com/4.18/docs/development/ui-development/touchgfx-engine-features/backend-communication

Side question: what user code might go into frontendapplication.cpp?

This topic has been closed for replies.