Skip to main content
franck23
Associate III
April 30, 2021
Solved

Is Graph "Precision" relevant when using float?

Hi,

I am trying to understand the graph "precision" as explained here:

https://support.touchgfx.com/docs/development/ui-development/ui-components/miscellaneous/dynamic-graph#precision

"If for example the level of precision is set to 0.1, each data point added to the DynamicGraph, will be multiplied by 10 internally"

I am using a histogram and giving the data points as floats.

I set the Precision to 1 and then to 0.1 but did not see any difference in the displayed value.

My data point is 20.0f.

I thought it would display a value of 200 with a precision set to 0.1.

Is the precision only used internally and not for display purposes?

Thanks for clarifying the use of this feature.

Franck.

This topic has been closed for replies.
Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
May 3, 2021

Hello franck23,

Yes the precision is done internally as specified in the link you shared.

To make it appear on the display you need to adapt your value range.

For example if you have a graph from 0 to 180 with a precision of 0.01, you will never see the difference.

But if you try with a range from 0 to 2 with a precision of 0.1 for example, you will see that it is more precise than precision 1.

Hope I clarified your doubts.

/Alexandre

2 replies

Alexandre RENOUX
Alexandre RENOUXBest answer
Visitor II
May 3, 2021

Hello franck23,

Yes the precision is done internally as specified in the link you shared.

To make it appear on the display you need to adapt your value range.

For example if you have a graph from 0 to 180 with a precision of 0.01, you will never see the difference.

But if you try with a range from 0 to 2 with a precision of 0.1 for example, you will see that it is more precise than precision 1.

Hope I clarified your doubts.

/Alexandre

franck23
franck23Author
Associate III
May 3, 2021

Hi Alexandre,

Thanks for the clarification.

It makes sense to me now.