Skip to main content
stan_av
Associate
Oct 9, 2018 6:46 PM UTC
Question

is dcmi from stm32L4 compatible with stm32L4+ ?

Is there a difference in the usage of the DCMI peripheral between the l4 (STM32L49x) microcontrollers and the l4+ (STM32L4R5xx) chips? 

I have a camera working with dma on dcmi with the STM32L496, but the same c code does not work correctly with STM32L4R5AG. Other peripherals (usb, gpios etc) work fine.

I find that instead of capturing a frame (in snapshot mode) the dcmi shows an overrun error with OVR_RIS set, and no frames are stored in the fifo or DMA memory location

Also which minimum CUBE version should be used ?

thanks

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Oct 10, 2018 4:04 AM UTC

I'd watch for differences in clocking structures, the rates of different buses, the dividers and PLL sources for different peripherals.

Review BSP of EVAL boards supporting camera connectivity.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
stan_av
stan_avAuthor
Associate
Oct 10, 2018 5:14 AM UTC

Thanks for the reply.

There does not seem to be an l4+ board with a dcmi project ..