Skip to main content
AndreaShim
Visitor II
January 4, 2022
Question

Is ADV7533 I2C Control necessary to work in ST B-LCDAD-HDMI1 DSI to HDMI adapter board?

Hi,

1) My development environment is as follows.

  HW : STM32f769ni discovery kit (DISCO) + ST + ST B-LCDAD-HDMI1 DSI + 7 INCH 1024*600 HDMI LCD

  SW : STM32CubeIDE + TOUCHGFX + TOUCHGFX DESIGNER

  I needed to replace embedded 4 inch touch LCD (DSI connector) with 7 INCH 1024*600 HDMI LCD. So I used ST B-LCDAD-HDMI1 DSI b'd which uses ADV7533 to convert from DSI to HDMI output.

2) The symptom is as follows.

  But there is no output on the 7 INCH 1024*600 HDMI LCD and "No Signal" message on the display

3) Question

 Do I need to set the corresponding display resolution, aspect ratio, working mode, ... in the ADV7533 using I2C ?  I only want to know whether it is necessary or not ?

 In case it it necessary, I don't want to know how to initialize those registers because I know that it is hard to know  even I2C Dev Address. I will try to find another LCDs & Interfaces

 In case it is not necessary, I'll try my best to find the corrent settings in the ST STM32CubeIDE Software.

Thanks for reading,

This topic has been closed for replies.