Skip to main content
AME MCU Support Center BB
ST Employee
Sep 27, 2019 5:11 PM UTC
Question

Interfacing with hardware in TouchGFX Applications - Example ported to TouchGFX Designer V4.10 and STM32CubeIDE

Hello,

I ported the first example in the article "Interfacing with hardware in TouchGFX Applications" to TouchGFX Designer V4.10 and then ported it to STM32CubeIDE V1.0.2.

Please find it in attachment. I hope you find it helpful.

I didn't use the ioc and I am not sure its gonna work.

Board: STM32F746G-DISCO

Tools:

IAR EWARM V8.40.1

STM32CubeIDE V1.0.2

STM32CubeProgrammer V2.1.0

Note: STM32CubeIDE doesn't load the assets to the external memory. You need STM32CubeProgrammer having the external loader "N25Q128A_STM32F746G-DISCO" selected to load the assets.

With regards,

Badreddine

This topic has been closed for replies.

3 replies

Martin KJELDSEN
Principal III
Sep 30, 2019 8:19 AM UTC

Hi @AME MCU Support Center BB​,

Thanks for the contribution!

/Martin

AME MCU Support Center BB
ST Employee
Sep 30, 2019 11:48 PM UTC

@Martin KJELDSEN​ No worries! I am trying to pay back :)

@All

I ported the second method (From other task) as well to STM32CubeIDE 1.0.2 and TouchGFX designer 4.10.

Please find it in attachment.