Skip to main content
Nicholas Yunker_2
Senior
May 20, 2025 9:51 PM UTC
Solved

Interfacing STM32H735G-DK w/ 7" screen using EK9713CA Driver IC

I started out by using the stock 4.3" display on the STM32H735G-DK Discovery Kit and with TouchGFX I was able to get a nice example project running.  Now I am attempting to interface a 7" 800x480 LCD panel with the kit.  This panel uses the EK9713CA driver IC.  The datasheet for the panel lists these timing characteristics:

NicholasYunker_2_0-1747777486354.png

Can some one please help me understand how to enter these into the LTDC configuration page on STM32CubeMX?  I've attempted to figure this out several different ways and I just keep getting a blank screen and the code just hangs during execution.  I suspect the issue is in the how I am entering these timings.



This topic has been closed for replies.
Nicholas Yunker_2
Senior
May 30, 2025 8:24 PM UTC

I managed to get a better datasheet/app note from the manufacturer that named the timings better.  From that I was able to get the timings correct and the screen to work.  Here is a screenshot of the .ioc file that shows the correct settings:

NicholasYunker_2_0-1748636594728.png

NicholasYunker_2_1-1748636617286.png

 

 

3 replies

Nicholas Yunker_2
Senior
May 21, 2025 3:39 PM UTC

I have stepped through my code and find that it hangs when it reaches the backPorchExited() function in the TouchGFXHAL.cpp file

madGambol
Associate
May 30, 2025 8:19 PM UTC

Nicholas,

Would you mind sharing your ioc file?

Thanks,

Chris

Nicholas Yunker_2
Nicholas Yunker_2AuthorBest answer
Senior
May 30, 2025 8:24 PM UTC

I managed to get a better datasheet/app note from the manufacturer that named the timings better.  From that I was able to get the timings correct and the screen to work.  Here is a screenshot of the .ioc file that shows the correct settings:

NicholasYunker_2_0-1748636594728.png

NicholasYunker_2_1-1748636617286.png