Skip to main content
Associate
Feb 15, 2025 3:36 PM UTC
Question

Improving Download Speed

Hello,

I am working on an application that is somewhat large and each time I upload to my Disco Board it is taking three to four minutes because all of the TouchGFX images are being re-generated and uploaded. Is there a way to only upload the code from XCUBE with the screens staying the same? This would greatly reduce my development time. 

Any help would be great. 

Thanks,
Alex

This topic has been closed for replies.

7 replies

Pavel A.
Feb 15, 2025 5:53 PM UTC

Yes it is possible to build your app so that content in the external memory is excluded. Make additional project configuration for this, like "Debug internal only" or "Release internal only". Search the forum, this has been asked before.

 

amspurgeAuthor
Associate
Feb 15, 2025 8:28 PM UTC

Got any links you could share?

Tesla DeLorean
Guru
Feb 15, 2025 7:31 PM UTC

Which DISCO board, they make a few.

Yes, would help if ST have some more robust processes for incremental build/update

The devices with ST-LINK/V3 run a lot faster. USB 2.0 HS helps, with right ports and cables

Writing multiple megabytes of QSPI NOR FLASH can be quite involved.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
amspurgeAuthor
Associate
Feb 15, 2025 8:30 PM UTC

I’m using the STM32F769I-DISCO. We were able to get from 3 min to 1:15 min by adjusting the settings. The problem seems to be that it spends over a minute searching for the STLink/Device. Any thoughts?

Osman SOYKURT
ST Technical Moderator
Feb 17, 2025 10:28 AM UTC

Hello @amspurge ,

Do you use TouchGFX Designer to run on target (F6)? Or maybe you compile with another compiler (like STM32CubeIDE), and flash using STM32CubeProgrammer?

ST Software Developer | TouchGFX
Osman SOYKURT
ST Technical Moderator
Feb 25, 2025 10:37 AM UTC

Hello @amspurge ,

Have you been able to move on with your issue?

ST Software Developer | TouchGFX