Skip to main content
cvinc.11
Visitor II
May 4, 2022 12:06 PM UTC
Question

Import GUI project and modify resolution

To use a GUI from one project on another board, I tried to "Import GUI" through TouchGFX from a project developed on STM32G071 into another STM32F429I board and it works,

The Import process on TouchGFX: Edit => Import GUI => BROWSE => exist project => Import

 The problems :  

- Graphic problem: The project remains in the dimensions of the initial board, there is no adaptation of the size of the Screens

-Code issue : Error: FLASH region overflowed by *** bytes => we have to reduce the size of the imported code, I tried to use compiler optimizations but it doesn't work.

 How can we fix it ?

Thanks

Regards

This topic has been closed for replies.

1 reply

MM..1
Super User
May 4, 2022 3:38 PM UTC

Duplicate TouchGFX GUI with another project (st.com)

but ok after import resolution is too imported. Save and close .

Edit in notepad template project or if in is ok resolution open template instead project .