Skip to main content
LMalv.1
Associate II
April 30, 2020
Question

II have STM32F7508-DK, I would like to integrate TouchGFX with STM32CUBE IDE, but it is not working, I am searching instructions or, even better, a tutorial. Thank you very much.

I have the development kit, I made an application, following an ST tutorial, but it is still not working. I have the .bin file, but when I debug the program the display doesn't show anything, and the red led continuos blinking, I think there are some problems programming the flash, but I do not know what to do to fix them.

This topic has been closed for replies.

5 replies

Martin KJELDSEN
Principal III
April 30, 2020

Can you try just opening the touchgfx designer, selecting F7508-DK and pressing "Run target"? It will use our makefiles (gcc) and stcubeprogrammer. Start by letting me know if that works for your board.

/Martin

LMalv.1
LMalv.1Author
Associate II
April 30, 2020

Thanks, using TouchGFX designer and run to target, works very well, but I would like to integrate teh project inside of STM32CUBE IDE.. Is that the problem

LMalv.1
LMalv.1Author
Associate II
April 30, 2020

Maybe, instead of integrating in STM32CUBE I can just make a TouchGFX project and read data from the UART. Do you think it will work?

Martin KJELDSEN
Principal III
April 30, 2020

Yes, no problem. The project supplied by the designer in order to run from within the designer is just a Makefile using gcc/arm-gcc to compile. You can modify it no problem if you want to get started immediately. I will have to find a board once i'm back at the office to test this

/Martin

Martin KJELDSEN
Principal III
April 30, 2020

I don't have a board with me right now so i can't check, but it shouldn't be a problem. The V3 templates support CubeMX generated projects.

/Martin