Skip to main content
MSale.1
Senior
September 24, 2020
Question

If i used the STM32H743 at 480 and the AHB bus at 240. will i be able to use the DCMI pixel clock at 96Mhz or its not possible at its fixed to 80Mhz even if the processor runs at 480Mhz

I have asked this question before and got no answer from STM so its better to clear it for us so we know

This topic has been closed for replies.

3 replies

ST Technical Moderator
September 24, 2020

Hello @Community member​ ,

According to the STM32H743 datahseet: max clock for DCMI is 80MHz. this data is the result of characterization.

Hope this answer your question.

Please select the post as a "Best Answer" if it answers your question.

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
MSale.1
MSale.1Author
Senior
September 24, 2020

@Imen DAHMEN​ 

Hi

In the datasheet its mentioned 80Mhz at 400Mhz. so even at 480Mhz the max will still be 80Mhz or 96Mhz?

CKUND.1
Associate II
September 24, 2020

The reference manual says on page 1187 (DCMI Clocks): "The maximum DCMI_PIXCLK period must be higher than 2.5 HCLK periods."

So, if AHB clock is 240 MHz / 96Mhz = 2.5

Maybe is possible to work, but you are trying to use the DCMI interface in the max clock possible. I don't know if is a good ideia!

Best Regards,

Kunde