Skip to main content
DMeis.1
Associate III
Feb 24, 2020 8:10 PM UTC
Question

I was wondering when the template for the ST32F7508 Disco kit to work with TouchGFX 4.13.0 would be out.

As the title says. I was in a webinar last week and I asked a question about the STM32F7508-Disco board not working with CubeIDE, CubeMX and TouchGFX. It is giving me memory errors when trying to load the code onto the board. They responded saying that the updated template would be released in about two weeks. Is there a way I will know when it is available?

Thanks!

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Feb 24, 2020 9:03 PM UTC

It is basically an STM32F746G-DISCO with less memory in the linker script. The die still has 1MB of FLASH, but you'd want to push as much as possible into the QSPI memories.

Subscribe to the TouchGFX forum/group, I'm sure they will announce a new version shortly. This week was going to be Embedded World, usually schedule big news for then. Two weeks is the usual number you give when things are reasonably imminent, and don't want to be queried every Friday..

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..