Skip to main content
mSH.1
Associate III
Jul 31, 2022 11:18 PM UTC
Question

I want to download the hexadecimal file of Proejct generated by touchGFX to the Discovery Board with STM32CubeProgrammer.

hello

I want to download the hexadecimal file of Proejct generated by touchGFX to the Discovery Board with STM32CubeProgrammer.

​

An operation has occurred.

​

  • used STM32H735G-DK ​/ CubeIDE
 08:16:59 : STM32CubeProgrammer API v2.9.0
 08:17:02 : ST-LINK SN : 004A001D3438510734313939
 08:17:02 : ST-LINK FW : V3J9M3
 08:17:02 : Board : STM32H735G-DK
 08:17:02 : Voltage : 3.28V
 08:17:02 : SWD freq : 24000 KHz
 08:17:02 : Connect mode: Normal
 08:17:02 : Reset mode : Software reset
 08:17:02 : Device ID : 0x483
 08:17:02 : Revision ID : Rev Z
 08:17:02 : ST-LINK SN : 004A001D3438510734313939
 08:17:02 : ST-LINK FW : V3J9M3
 08:17:02 : Board : STM32H735G-DK
 08:17:02 : Voltage : 3.28V
 08:17:02 : SWD freq : 24000 KHz
 08:17:02 : Connect mode: Normal
 08:17:02 : Reset mode : Software reset
 08:17:02 : Device ID : 0x483
 08:17:02 : Revision ID : Rev Z
 08:17:02 : Debug in Low Power mode is not supported for this device.
 08:17:02 : UPLOADING OPTION BYTES DATA ...
 08:17:02 : Bank : 0x00
 08:17:02 : Address : 0x5200201c
 08:17:02 : Size : 92 Bytes
 08:17:02 : UPLOADING ...
 08:17:02 : Size : 1024 Bytes
 08:17:02 : Address : 0x8000000
 08:17:02 : Read progress:
 08:17:02 : Data read successfully
 08:17:02 : Time elapsed during the read operation is: 00:00:00.002
 08:17:07 : Read File: C:\TouchGFXProjects\Noble_cooker\STM32CubeIDE\Debug\STM32H735G-DK.hex
 08:17:07 : Number of segments: 2
 08:17:07 : segment[0]: address= 0x8000000, size= 0x5DA00
 08:17:07 : segment[1]: address= 0x90000000, size= 0x86691C
 08:17:15 : Memory Programming ...
 08:17:15 : Opening and parsing file: STM32H735G-DK.hex
 08:17:15 : File : STM32H735G-DK.hex
 08:17:15 : Size : 9192220 Bytes
 08:17:15 : Address : 0x08000000 
 08:17:15 : Erasing memory corresponding to segment 0:
 08:17:15 : Erasing internal memory sectors [0 2]
 08:17:18 : Erasing memory corresponding to segment 1:
 08:17:18 : Download in Progress:
 08:17:21 : Error: failed to download Segment[1]
 08:17:21 : Error: failed to download the File

​thank.

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Jul 31, 2022 11:38 PM UTC

Make sure you've selected a suitable External Loader for the board, see [EL] gear/bitcoin icon on the lower left edge of the screen.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
Jul 31, 2022 11:52 PM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..