Skip to main content
Ebun.1
Senior
June 11, 2020
Solved

I want to create a parameter setting screen

Thank you for helping.

environment:

STM32F769I-DISCO

TouchGFX4.12.3

STM32CubeIDE1.3.0

I want to create a screen for setting parameters such as IP address.

(1)Is there a text box to enter in the UI? If not, how can this be achieved?

(2) How can you display the cursor?

(3) What is the method for displaying the keyboard on the screen and inputting?

Do you have a sample project?

Thank you.

This topic has been closed for replies.
Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
June 19, 2020

Hi,

The keyboard demo does not have a cursor implemented. You could create one by using a box widget and making it move accordingly to what you want.

What do you mean by focus on a text box?

I am currently working on a demo of a cursor with text/numbers that you can add/remove where you want. It might be useful to you, here is the link to the zip on wetransfer (couldnt load it directly to this message, so this is a temporary link). For now only screen 2 works so look only at the code related to screen2view.

/Romain

7 replies

Alexandre RENOUX
Visitor II
June 12, 2020

Hello,

You can find a Keyboard Example as well as Text Examples available in TouchGFX Designer.

/Alexandre

Ebun.1
Ebun.1Author
Senior
June 16, 2020

Thank you for your reply.

Why doesn't the designer see the keyboard screen?

How do you design it?

Alexandre RENOUX
Visitor II
June 16, 2020

Hello,

The Keyboard is not available in the Designer View in itself. It is hardcoded so you have to go through the code to see how it's implemented.

/Alexandre

Ebun.1
Ebun.1Author
Senior
June 19, 2020

Thank you for your reply.

How can I focus on a text box?

How can I display the cursor?

Do you have sample code?