Skip to main content
Ebun.1
Senior
Dec 24, 2019 6:26 AM UTC
Question

I want to change the resolution

Hello

​

In the case of F746-DISCO, the resolution is 480 × 272,

For example, how to customize when connecting 800x600 LCD?

​

Thank you.​

This topic has been closed for replies.

5 replies

HP_it
Senior II
Dec 25, 2019 12:46 PM UTC

TouchGFX derives the screen resolution from the LTDC interface setup. if you change it there it should change for the TouchGFX as well.

Ebun.1
Ebun.1Author
Senior
Dec 25, 2019 10:51 PM UTC

Hello HP's

OK.

Thank you for your response.

Bob Bailey
Senior
Dec 31, 2019 6:12 PM UTC

Did this work? I will be doing a similar change soon.

I presume the LCD's ribbons are soldered to the Disco board (I have not looked). Did you install a connector?

Bob

HP_it
Senior II
Jan 2, 2020 8:44 AM UTC

There's no connector under the screen - it's soldered directly on the board. I've looked. Also, the connector is really wide, like 1mm pitch or similar, so soldering on a connector is not trivial.