Skip to main content
MLuis.1
Associate III
Apr 19, 2023 11:11 AM UTC
Question

I'm implementing TouchGFX on a Custom BoardI detected that the RAM DQS Pin(OCSPI2_DQS) is always low and does not work.

I'm implementing TouchGFX on a Custom Board using the same circuit as the STM32H735G-DK for the external memories. I detected that the RAM DQS Pin(OCSPI2_DQS) is always low and does not work. The display is always grey as the framebuffer is not written properly.

The display is working well, I tested it by using an internal framebuffer.

My project is attached.

This topic has been closed for replies.

2 replies

Apr 19, 2023 11:38 AM UTC

Post link deleted to adhere community guidelines.

MLuis.1
MLuis.1Author
Associate III
Apr 19, 2023 11:47 AM UTC

The hardware is all correct in terms of the circuit. I checked all the lines with an appropriate oscilloscope and all are working fine except for the DQS on the RAM. All the memory components are the same as the STM32H735G-DK board as well as the firmware configuration.