Skip to main content
MSale.1
Senior
June 16, 2020
Question

I have application with Two layers first layer for live video and the second for the gui. the camera buffer in external sdram and the gui in internal ram but i have pixel distortion in gui. what might cause it?

I have doubt that the bandwidth of the internal memory which is 1536MB/s is too fast. i am using stm32h743 at 480 MHz and the AXI bus speed is 240MHz.

This topic has been closed for replies.

11 replies

MSale.1
MSale.1Author
Senior
June 16, 2020

Problem was solved

Alexandre RENOUX
Visitor II
June 16, 2020

Good =)

Can you explain how you solved it ? It might help others.

Thank you in advance.

/Alexandre

MSale.1
MSale.1Author
Senior
June 24, 2020

@Alexandre RENOUX​ 

Hi,

Sorry for late reply. i disabled the cache which solved the problem.

I have another question. how can i Create a loader for parallel nor flash to store the assets there?

Regards

Mahmoud