Skip to main content
EGord.2
Visitor II
Jul 25, 2022 12:03 PM UTC
Question

i cant get RAW imagenes in stmf429

Hi everyone

I,m having a problem when i try to capture a photo in raw format with the OV5640 camera. I get an image of a suitable size but it adds the header of the JPEG that i want to avoid it.

When i try to open it with the image viewer, i can see the image but it has wrong colors.

I,m using ADC with DMA in Snapshot and when i starting the DCMI i have JPEGMode = DMI_JPEG_DISABLE

anyone can help me?

Thank you in advance

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
Jul 25, 2022 12:06 PM UTC

Pretty sure that information is coming from the camera, check what settings are in that, not the STM32

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..