Skip to main content
q123w123e123qweqwe
Associate III
May 28, 2020
Question

I cant detect touch on STM32f746. I'm using stmpe811 for touch controller

Hello,

I'm working on a project an using STM32F746 and STMPE811 for touch controller. I did initializations and everything but no metter hjow much try I can't detect touch. Also I con't do debugging step by step because my code always goes into TIM6_DAC_IRQHandler() funtion. and come back to where it was. it do not go to next line(only if I try debug step by step). So can anyone help me with these issues?

Thank you.

bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y)
{
 if (tsDriver)
 {
 //In here DetectTouch's value is always 0x80060c3 Idk why
 if (tsDriver->DetectTouch(TS_I2C_ADDRESS))
 {
 /* Get each touch coordinates */
 tsDriver->GetXY(TS_I2C_ADDRESS, (uint16_t*)&y, (uint16_t*)&x);
 return true;
 }
 }
 return false;
}

This topic has been closed for replies.

2 replies

Martin KJELDSEN
Principal III
May 28, 2020

How did you create this project? The code looks like something we wrote for the Touch Controller in the latest application template.

/Martin

q123w123e123qweqwe
Associate III
May 28, 2020

I’ve got it from template project for STM32F429 discovery. Because as I said I’m using stmpe811. So integrated it to stm32f746 custom project. Was it a bad idea?