Skip to main content
MKoca.1
Senior
Sep 9, 2024 12:56 PM UTC
Question

I CANNOT WRITE DATA TO EXTERNAL FLASH WHILE STM32H750 TOUCHGFX IS RUNNING

STM32H750 EXTERNAL FLASH WRITE DATA PROBLEM

Hello everyone,
I am working on a TouchGFX project using STM32H750. In order for the program to be executed, I started the program on the external flash at address 0x90000000 using the bootloader. My project works perfectly for now and I can do everything I want via TouchGFX. I use a 10.1 inch screen. I use MT25QL512ABB8ESF as an external flash and IS42S32400F-6TL as an external RAM. My real problem starts from here. In the later stages of the project, I want to write different data to the external flash whenever I want. And I also want to update the application via WiFi or USB. In order to do these, I need to be able to write data to the external flash while TouchGFX is running. I haven't figured out how to do this yet. Can you help me with this?

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
Sep 9, 2024 1:10 PM UTC

It's going to be a challenge, as you can't concurrently memory-map / XIP and send commands and stall for erase and writes.

You'll need to create a subsystem that runs under Internal Flash, or RAM

Can you stage to something else, like MicroSD / eMMC or secondary SPI attached NOR FLASH, or NAND FLASH

If staged you can deal with updates at start-up before running the main application.

Perhaps if you don't memory-map, and rather use the QSPI as a Flash File system, pulling image data via RAM as needed. You'll need to look at different modes of operation TouchGFX can use to load/resource. Or an update screen where very limited functionality the suspends memory-mapped operation.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MKoca.1
MKoca.1Author
Senior
Sep 9, 2024 1:21 PM UTC

Thank you for your quick response, sir.
Frankly, I have come across a few topics on the forum about writing data to flash in a very limited functionality state that disables interrupts and suspends memory-mapped operations. At least the application update can be done this way, I can lock the update screen and block the user until the update is finished. However, I could not figure out how to program a very limited functionality state that disables interrupts and suspends memory-mapped operations. An example of this would be very useful.

Tesla DeLorean
Guru
Sep 9, 2024 1:33 PM UTC

>>An example of this would be very useful.

I'd imagine, perhaps you can get the ST / TouchGFX team, or your FAE to work on that.

 

Another alternative via USB, is that you come up a solely a USB MSC, and a portion of the QSPI FLASH can be provided to be a FLASH DRIVE so the user can drag-n-drop update files, which can be processed once the drive is disconnected.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..