Skip to main content
RBoud.1
Associate II
Dec 5, 2022 10:28 AM UTC
Question

I am using STM32F446RTE (64pins) with TouchGFX 4.18. The screen is working but there is slight flickering (slow refresh time). As I don't need touch screen function, can I stop continuous refreshing of the screen and only update the screen where need

..

This topic has been closed for replies.

2 replies

MM..1
Super User
Dec 5, 2022 12:41 PM UTC

touch screen function isnt relevant to this

yes if you have display with memory

RBoud.1
RBoud.1Author
Associate II
Dec 5, 2022 2:00 PM UTC

Excellent, thank you. uController has 512KB flash and 128KB Ram. Program mem usage is Program Size: Code=140840 RO-data=96468 RW-data=580 ZI-data=46596. TouchGFX use partial mode. How can I achieve this or which TouchGFX function to call to refresh the screen? I Want to use flags to call this function.