Skip to main content
JRuss.5
Associate
Aug 11, 2022 8:46 PM UTC
Question

I am planning on using the STM32G070, a small 240 x 240 LCD Display and external NOR Flash with TouchGFX. Can I perform DMA Transfers directly from the external NOR Flash Memory to the Display memory? Thanks, Jim Russell

..

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Aug 11, 2022 8:51 PM UTC

I believe it should work with DMA in the same manner internal FLASH would, only slower.

You can't concurrently write into NOR Flash and read it, or memory map to it. So generally whatever you have in Flash will be static.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JRuss.5
JRuss.5Author
Associate
Aug 15, 2022 11:16 PM UTC

I was only planning to use NOR Memory DMA Transfers for full screen updates. Thanks.