Skip to main content
Junde
Senior III
Jun 13, 2024 3:30 PM UTC
Solved

How to write/draw something in my screen by touchGFX?

Hello there,

I want to recognize the digital and character written by hand with STM32F429BI.

I think there must be split into the following steps:

1. user input(write something in the screen by finger); (what widget I can use?)

2. transfer the screen pixel data to MCU from touchGFX; (How to get the partial pixel data in certain areas?)

3. MCU recognizes the content with some lib; (Can some Lib be used from ST?)

4. MCU sends the result to the screen for display; (I know how to do this only :face_with_tears_of_joy:)

Any advice and links are expected.

Thanks for your help.

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
Jun 14, 2024 9:03 AM UTC

Hello @Junde ,

 

1) user input(write something in the screen by finger); (what widget I can use?)
The best widget to use seems to be the canvas widget .
It is better to use this than to add a 1x1 box because you are limited in memory (and therefore limited in the amount of elements you can add).
You could get the position of the finder with the drag event or the handledragevent directly from the widget itself.
You could save the last position of the finger and draw a line between that last position and the current position. This would give you a boxy but simple implementation.
If you want to do things better, you can use 4 points instead of 2 to get a smoother curve using the quadraticbezierto() method.

2) transfer the screen pixel data to MCU from touchGFX; (How to get the partial pixel data in certain areas?)
You can get the framebuffer data by checking where you store the framebuffer.
Open your STM32CubeMX file (in your project folder, open the .ioc file), check "middleware", then "TouchGFX" and here you can see where your framebuffer is stored :

GaetanGodart_0-1718355323409.png

Your framebuffer size id width*height*RGBprecision. Here is another example of that : memory-consumption .

Now that you have the framebuffer location and size, you need to only fetch the data of the canvas (or alternatively you could isolate the drawing by saving the minX, minY, maxX and maxY and adding a bit of padding) and store it into whatever format you want (an array, a jpeg, a png, a bmp).

3) MCU recognizes the content with some lib; (Can some Lib be used from ST?)
It is up to you to do that research.
The first link on google mentions tesseract. I have personally used tesseract in Python and it worked fine (also exist in c++).

 

I hope this guidance is enough.

 

If this comment answers your problem, I invite you to select it as "best answer".
Otherwise, don't hesitate to specify where you are stuck.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)

15 replies

MM..1
Super User
Jun 13, 2024 4:14 PM UTC

I mean nothink prepared for this freely exist, you can create custom widget and use canvas...Custom Widgets | TouchGFX Documentation

Junde
JundeAuthor
Senior III
Jun 14, 2024 9:53 AM UTC

@MM..1 

Thanks for your help, I will try it later!

GaetanGodart
GaetanGodartBest answer
ST Employee
Jun 14, 2024 9:03 AM UTC

Hello @Junde ,

 

1) user input(write something in the screen by finger); (what widget I can use?)
The best widget to use seems to be the canvas widget .
It is better to use this than to add a 1x1 box because you are limited in memory (and therefore limited in the amount of elements you can add).
You could get the position of the finder with the drag event or the handledragevent directly from the widget itself.
You could save the last position of the finger and draw a line between that last position and the current position. This would give you a boxy but simple implementation.
If you want to do things better, you can use 4 points instead of 2 to get a smoother curve using the quadraticbezierto() method.

2) transfer the screen pixel data to MCU from touchGFX; (How to get the partial pixel data in certain areas?)
You can get the framebuffer data by checking where you store the framebuffer.
Open your STM32CubeMX file (in your project folder, open the .ioc file), check "middleware", then "TouchGFX" and here you can see where your framebuffer is stored :

GaetanGodart_0-1718355323409.png

Your framebuffer size id width*height*RGBprecision. Here is another example of that : memory-consumption .

Now that you have the framebuffer location and size, you need to only fetch the data of the canvas (or alternatively you could isolate the drawing by saving the minX, minY, maxX and maxY and adding a bit of padding) and store it into whatever format you want (an array, a jpeg, a png, a bmp).

3) MCU recognizes the content with some lib; (Can some Lib be used from ST?)
It is up to you to do that research.
The first link on google mentions tesseract. I have personally used tesseract in Python and it worked fine (also exist in c++).

 

I hope this guidance is enough.

 

If this comment answers your problem, I invite you to select it as "best answer".
Otherwise, don't hesitate to specify where you are stuck.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Junde
JundeAuthor
Senior III
Jun 14, 2024 9:53 AM UTC

@GaetanGodart 

So many thanks to you for your detailed answer.

I will verify the "canvas widget" later, seems it can work well for my requirements.

I am trying to do it by LTDC Layer2, and I can draw something now.

As you said, it needs more RAM for the layer2 area.

Junde
JundeAuthor
Senior III
Jun 18, 2024 6:38 PM UTC

Hi @MM..1 @GaetanGodart 

Many thanks for your pieces of advice and support.

Finally, I get the way!

The canvas line needs too much RAM, so I give it up.

I returned to the LTDC second layer(I think it's similar to the TouchGFX bitmap)

After some tries, it finally worked well.

I uploaded the project HERE for anyone wanting to have a reference.