Skip to main content
hlian.1
Associate II
June 5, 2020
Question

How to use 8pp to drive rgb565lcd (via STM32 ltdc controller)

Hello Martin,

My platform is stm32l4r7zi, which uses ltdc to drive 800 × 480 LCD in the way of rgb565 connection. Because the internal RAM (640kb) is not large enough for frame buffer, so I want to select 8bit color depth in the touch designer. Can this method be implemented? Does ltdc need to be configured in L8 format?

Thank you.

This topic has been closed for replies.

8 replies

Romain DIELEMAN
ST Employee
June 8, 2020

Hi,

this process would have to be done in your board configuration and settings rather than TouchGFX Designer. Are you using CubeMX by any chance?

To reduce the usage of RAM have you considered using partial frame buffers instead ? It does lower the performances a bit but if you are not doing full screen updates or complex 3D animations, this could be your solution.

/Romain

Breeze1
Associate III
June 8, 2020

https://support.touchgfx.com/docs/development/ui-development/scenarios/lowering-memory-usage-with-partial-framebuffer/

This says :

  • Partial frame buffers will only work on displays that have built-in memory. These are typically DSI displays or displays with a parallel bus connection (DBI type A/B, 8080/6800) or SPI-bus connection.
  • Potential tearing for complex applications.

LTDC interface ,but not with DSI, how to use partial frame bufffer?

Romain DIELEMAN
ST Employee
June 9, 2020

Arh it is my bad I didn't read carefully your setup :sad_but_relieved_face: ... It is not possible with LTDC since you transfer directly the frame buffer to the display and not go through its internal memory.

But there is a section on l8 images in the doc that might help you.

hlian.1
hlian.1Author
Associate II
June 8, 2020

thank you Romain ,I will try  partial frame buffers

Breeze1
Associate III
June 15, 2020

@Martin KJELDSEN​ 

Realy hoping for your answer

Martin KJELDSEN
Principal III
June 15, 2020

I don't understand the sentence "LTDC interface ,but not with DSI, how to use partial frame bufffer?" - Are you asking how to use partial framebuffers with LTDC?

Breeze1
Associate III
June 15, 2020

Actually yes, we are using a screen which has LTDC interface, but the screen do not have internal memory. We find it not possible to use partial frame buffer. Then We want to use L8 pix format to save RAM, but touch designer do not have L8 pix format . Looks like touch designer only support L8 pix format picture or Bitmap? So we set touch desinger to ARGB2222, which is as long as L8. We can transfer ARGB2222 to L8 using a few codes. But touch designer do not write data to framBuffer, waht can I do?