Skip to main content
Associate III
Aug 29, 2024 7:08 AM UTC
Question

How to update TouchGFX LCD setting in STM32H747I DISO ?

Dear Sir,

My  STM32H747I DISO board's LCD is MB1166-A09 , it's driver is nt35510. When I use "STM32H747I DISO board" to create new project, the lcd driver is otm8009a. May I change the default driver to nt35510 ?

 

Thanks.

This topic has been closed for replies.

3 replies

ST Employee
Aug 29, 2024 2:58 PM UTC

Hello @Kenwang,

Of course, you can change the provided configurations as you wish. To do so, you need to replace the drivers for otm8009a with nt35510, and also reflect the required changes in main.c and main.h.

I hope this helps you!

Mohammad MORADIST Software Developer | TouchGFX
KenwangAuthor
Associate III
Aug 29, 2024 3:44 PM UTC

Thanks for your reply.

Could you tell me how to replace main.c and main.h ? Which directory are they in?

ST Employee
Aug 30, 2024 8:59 AM UTC

When you create a STM32H747I-Disco project from TouchGFX designer, you will have a project directory structure as below. Navigating through CM7->Core you can find main.c inside Src and main.h in Inc. Please, study the code and how the display driver is used before replacing it with nt35510. 

STM32H747I-Disco TouchGFX Board SetupSTM32H747I-Disco TouchGFX Board Setup

Project Directory StructureProject Directory Structure

 

Mohammad MORADIST Software Developer | TouchGFX