Skip to main content
JLee.32
Associate III
May 13, 2021
Question

How to shorten the programming flash time for a project with TouchGFX?

MCU: STM32H750

IDE: STM32CubeIDE

Due to lots of image files for UI, I need to spend around 3~4 minutes programming the external flash. Can I specify a code area and an image area for the external flash? Then if image files are not changed, can I just update the code area?

Or is there any way to shorten the programming flash time for a project with TouchGFX?

This topic has been closed for replies.

2 replies

Romain DIELEMAN
ST Employee
May 27, 2021

Hi,

I guess you are looking for something like this video made by HP.

/Romain

JLee.32
JLee.32Author
Associate III
May 28, 2021

The externalFlash of my project includes app code and graphics. The internal flash only has boot code. Therefore, in order to debug hardware interaction, I still need to flash the externalFlash. It seems the video put the app code in the internal flash, and put the graphics (or touchgfx related) in the external flash. Is that correct? If so, could you show me how to do this?