Skip to main content
GMeur
Associate III
May 20, 2019 8:45 AM UTC
Solved

How to set the color of a button from code?

Hello,

Is there a way to change the color of a botton directly from the code?

Thanks.

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
May 20, 2019 9:00 AM UTC

Hi @GMeur​,

There are multiple types of buttons. If you're using a standard Button it requires an image for both released and pressed states so you would have to have assets in the color of your choice.

If you're using a flex button, you might be using a "Box with Border" - And here you can change the color of the box (and thus button) directly.

/Martin

3 replies

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
May 20, 2019 9:00 AM UTC

Hi @GMeur​,

There are multiple types of buttons. If you're using a standard Button it requires an image for both released and pressed states so you would have to have assets in the color of your choice.

If you're using a flex button, you might be using a "Box with Border" - And here you can change the color of the box (and thus button) directly.

/Martin

GMeur
GMeurAuthor
Associate III
May 20, 2019 9:28 AM UTC

Thanks for your quick reply.

Therefore, if I want to design a keyboard whose color of the keys can be changed easily from the code, I must use flex buttons for them and implement the 'clicklistener' function, right? Can you think of any easier ways of doing it?