Skip to main content
Michael B
Associate III
Jul 20, 2019 2:54 AM UTC
Solved

How to scaffold new projects from environment command line?

I'm just getting back into this after taking a 2 year break. I vaguely remember you could scaffold new projects from the command line rather than using the Designer application. I couldn't find any docs on this, is it still possible to do or am I completely mistaken?

This topic has been closed for replies.
Anders Nedergaard PETERSEN
Senior II
Jul 22, 2019 6:47 AM UTC

hi @Community member​,

The "new" normal way of creating a TouchGFX project is through the Designer.

We are also shipping a command line tool which does exactly what you describe :)

it is called tgfx.exe and is placed in the same installation folder as the designer.

Here is a snippet of the "help" context from the new command:

'new' - Combines a user interface with an application template to create a new application

Expected usage: tgfx.exe new <options>

<options> available:

   --ui=VALUE       Gui package name

   --at=VALUE       At package name

   --out=VALUE      Output Directory

   --prj=VALUE      Project Name

There is just one small catch, if you want to create any other projects than an empty application for pc simulator, you have to use the Designer to first download the desired Application Template and UI packages.

/Anders

2 replies

Anders Nedergaard PETERSEN
Senior II
Jul 22, 2019 6:47 AM UTC

hi @Community member​,

The "new" normal way of creating a TouchGFX project is through the Designer.

We are also shipping a command line tool which does exactly what you describe :)

it is called tgfx.exe and is placed in the same installation folder as the designer.

Here is a snippet of the "help" context from the new command:

'new' - Combines a user interface with an application template to create a new application

Expected usage: tgfx.exe new <options>

<options> available:

   --ui=VALUE       Gui package name

   --at=VALUE       At package name

   --out=VALUE      Output Directory

   --prj=VALUE      Project Name

There is just one small catch, if you want to create any other projects than an empty application for pc simulator, you have to use the Designer to first download the desired Application Template and UI packages.

/Anders

Michael B
Michael BAuthor
Associate III
Jul 25, 2019 10:58 PM UTC

Seems like an acceptable catch - I do like the designer in general but this is great information. Thanks!