Skip to main content
manto.1
Associate III
Aug 2, 2022 10:04 AM UTC
Question

How to save an image in different section then ExtFlashSection

This code works OK and is an example of an image that is not stored in sectionExtFlashSection.

// Generated by imageconverter. Please, do not edit!
 
#include <touchgfx/hal/Config.hpp>
 
 
//LOCATION_PRAGMA("ExtFlashSection")
//KEEP extern const unsigned char image_piklogo[] LOCATION_ATTRIBUTE("ExtFlashSection") = // 800x480 RGB888 pixels.
LOCATION_PRAGMA("LogoSection")
KEEP extern const unsigned char image_piklogo[] LOCATION_ATTRIBUTE("LogoSection") = // 800x480 RGB888 pixels.
{
 0xFF, 0xFF, 0x00, 0xFF, 0x00, 0x00, 0xFF, 0x00, 0xFF, 0x00, 0x00, 0x00,

The problem is that this code is rewriten every time I generate code in TouchGFX designer.

Is there a different way to achive what I want.

This topic has been closed for replies.

1 reply

MM..1
Super User
Aug 2, 2022 12:09 PM UTC

Learn use LD linker file script and place arangement for imagepiklogo.o here. I mean this file isnt regenerated.