Associate II
Jun 28, 2024 12:05 AM UTC
Solved
how to run STM32Cube.ioc at TouchGFX project?
- 1 reply
- 972 views
Hi I am luis.
I'm testing TouchGFX, and I have a question.
After creating an example board project with TouchGFX V4.22.1 Designer and then moving the STM32F769I_DISCO.ioc file into the STM32CubeIDE folder to set the IO, an error occurs when compiling after setting the IO. There are too many errors to easily resolve. I would like to know what is the optimal way to set up IO after creating a project with TouchGFX V4.22.1 Designer.