Skip to main content
Chi
Associate II
Jan 17, 2019 2:57 AM UTC
Solved

How to reuse a Custom Container in a new TouchGFX project

​Hi all, it seems that simply copying related files to path doesn't work and the reason is likely to be that the widget hasn't been registered in the new project yet. Wondering how to do the grafting work correctly.

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Jan 24, 2019 1:53 PM UTC

Hi @Chi​ ,

Currently there's no way to directly copy just a Custom container from the designer to another project. You have to import an entire gui from another .touchgfx file. I think it's something we'd like to make easier.

Your only option is to create it again, or to simply copy the generated code to your new project and rename the class (From MyCustomContainerBase to something else) and use that as code in your concrete views. If it's not too complex, i'd remake it. Or you can snip the code from the .touchgfx file if you can identify it. But i will bring this topic up again!

Thanks,

Best regard,

Martin

2 replies

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Jan 24, 2019 1:53 PM UTC

Hi @Chi​ ,

Currently there's no way to directly copy just a Custom container from the designer to another project. You have to import an entire gui from another .touchgfx file. I think it's something we'd like to make easier.

Your only option is to create it again, or to simply copy the generated code to your new project and rename the class (From MyCustomContainerBase to something else) and use that as code in your concrete views. If it's not too complex, i'd remake it. Or you can snip the code from the .touchgfx file if you can identify it. But i will bring this topic up again!

Thanks,

Best regard,

Martin

Associate III
Mar 14, 2024 2:56 PM UTC

Has there been any updates on this matter?