Skip to main content
KNara.2
Associate III
Mar 30, 2023 6:12 AM UTC
Question

How to resize the width and height of progress bar?

I'm looking for customising the progress bar width to 344 and height to 20.

Is there a way of customising the background image of the progress bar?

This topic has been closed for replies.

4 replies

Romain DIELEMAN
ST Employee
Mar 30, 2023 7:18 AM UTC

Hi,

The progress bar widget uses an image as a background. You cannot change the width or height of this image from TouchGFX Designer. The solution is to use another image with the size you are looking for (you could for example just take the one currently used and edit it in paint.net.

/Romain

KNara.2
KNara.2Author
Associate III
May 5, 2023 9:15 AM UTC

Hi @Romain DIELEMAN​ 

Got it.

What about the progress indicator?

How do I a customise that according to the background image.

I do not see any option of choosing the progress indicator.

To be more specific I'm using the box progress indicator and need the progress indicator edges to be curved ( same as the background image). How can I achieve this?

Yoann KLEIN
ST Employee
May 10, 2023 2:29 PM UTC

Hello @KNara.2​,

BoxProgress widget with rounded corners is not supported natively in TouchGFX.

But it should be possible to do it (not easy though), by modifying the framework code inside your project.

You'll have to modify the BoxProgress.hpp file, located inside "yourproject/touchgfx/framework/containers/progress_indicators/".

You can round the corners by creating Circle widgets and positioning them on the corners of your box.

We did almost this, some months ago, with a Button widget. For that, we modified the BoxWithBorderButtonStyle.hpp file. I'll share it so you can get some inspiration on how to achieve what you want.

Hope it helps,

/Yoann

Yoann KLEINST Software Developer | TouchGFX
Graduate II
May 10, 2023 7:54 PM UTC

Thank you Yoann for inspiration to get round corner flex buttons. I little bit continue it to get different colors for border and background. Now It seems to work pretty nicely with short testing. One question, is there any way to select painter automatically for different color setups (RGB888,565 etc) ?