Skip to main content
Zlian.1
Associate II
May 28, 2021
Question

How to realize touchgfx display in stm32l4r9 using OSPI memory mapping mode?

  1. The flash loader has been successfully made.
  2. The OSPI memory mapping mode has been verified successfully.

Question:

When touchgfx designer selects extflash, the screen is black, and it is normal to switch to intflash。。。。

I feel incredible,can't find out the cause of the problem:tired_face:

Do I need to modify any files of touchgfx?

​

***.sct​:

LR_IROM1 0x08000000 0x00200000 {  ; load region size_region

 ER_IROM1 0x08000000 0x00200000 { ; load address = execution address

  *.o (RESET, +First)

  *(InRoot$$Sections)

  .ANY (+RO)

 }

 RW_IRAM1 0x20000000 0x00040000 { ; RW data

  .ANY (+RW +ZI)

 }

 RW_FRAMEBUFFER 0x20040000 UNINIT 0x00060000 { ; RW data framebuffer

  ; Allocating region to framebuffer

 }  

}

​

LR_EROM1 0x90000000 0x4000000 {  ; load region size_region

 ER_EROM1 0x90000000 0x4000000 { ; load address = execution address

  *.o (ExtFlashSection)

  *.o (TextFlashSection)

  *.o (FontFlashSection)

 }

}

​

​

This topic has been closed for replies.