Skip to main content
MSale.1
Senior
Jul 9, 2020 1:14 PM UTC
Question

How to measure MCU Load while using TouchGFX?

..

This topic has been closed for replies.

2 replies

Alexandre RENOUX
Visitor II
Jul 9, 2020 1:55 PM UTC

Hello,

You can refer to any Application Template available on TouchGFX Designer but for instance you can look at the Application Template STM32F746G-DISCO with the TouchGFX Demo 1. This will tell you how both on the hardware development and GUI development side you implement the MCU load.

/Alexandre

Martin KJELDSEN
Principal III
Jul 17, 2020 11:55 AM UTC

Here's a few extra pointers to look for in any of the demos that Alexandre mentioned.

This code is required in FreeRTOSConfig.h

/* USER CODE BEGIN Defines */
/* Section where parameter definitions can be added (for instance, to override default ones in FreeRTOS.h) */
#define traceTASK_SWITCHED_OUT() xTaskCallApplicationTaskHook( pxCurrentTCB, (void*)1 )
#define traceTASK_SWITCHED_IN() xTaskCallApplicationTaskHook( pxCurrentTCB, (void*)0 )
/* USER CODE END Defines */

If you're using FreeRTOS - this code is required in your OSWrappers.cpp. We don't have examples for other OS.

// FreeRTOS specific handlers
extern "C"
{
 void vApplicationStackOverflowHook(xTaskHandle xTask,
 signed portCHAR* pcTaskName)
 {
 while (1);
 }
 
 void vApplicationMallocFailedHook(xTaskHandle xTask,
 signed portCHAR* pcTaskName)
 {
 while (1);
 }
 
 void vApplicationIdleHook(void)
 {
 // Set task tag in order to have the "IdleTaskHook" function called when the idle task is
 // switched in/out. Used solely for measuring MCU load, and can be removed if MCU load
 // readout is not needed.
 vTaskSetApplicationTaskTag(NULL, IdleTaskHook);
 }
}

Then some MCU Instrumentation is required in order to get the clocl cycle count for a particular MCU family, in this case F7 - TouchGFX HAL will call these functions if instrumentation is configured.

#include <bsp/STM32F7Instrumentation.hpp>
#include <touchgfx/hal/HAL.hpp>
 
extern "C"
{
#include "stm32756g_eval_sdram.h"
#include "stm32756g_eval_lcd.h"
#include "stm32756g_eval_io.h"
#include "stm32756g_eval_nor.h"
#include "stm32f7xx_hal_dma.h"
#include "stm32f7xx_hal_qspi.h"
#include "stm32f7xx_hal_rcc_ex.h"
#include "stm32f7xx_hal_tim.h"
}
namespace touchgfx
{
TIM_HandleTypeDef tim;
 
void STM32F7Instrumentation::init()
{
 __TIM2_CLK_ENABLE();
 tim.Instance = TIM2;
 tim.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 tim.Init.CounterMode = TIM_COUNTERMODE_UP;
 tim.Init.Period = 0xFFFFFFFF;
 tim.Init.Prescaler = 0;
 tim.Init.RepetitionCounter = 1;
 HAL_TIM_Base_Init(&tim);
 HAL_TIM_Base_Start(&tim);
}
 
//Board specific clockfrequency
unsigned int STM32F7Instrumentation::getElapsedUS(unsigned int start, unsigned int now, unsigned int clockfrequency)
{
 return ((now - start) + (clockfrequency / 2)) / clockfrequency;
}
 
 
unsigned int STM32F7Instrumentation::getCPUCycles()
{
 return __HAL_TIM_GET_COUNTER(&tim);
}
 
void STM32F7Instrumentation::setMCUActive(bool active)
{
 if (active) //idle task sched out
 {
 cc_consumed += getCPUCycles() - cc_in;
 }
 else //idle task sched in
 {
 cc_in = getCPUCycles();
 }
}
}