Skip to main content
Btovi.1
Associate
Dec 7, 2020 5:41 PM UTC
Question

How to load Touchgfx files to external flash

I have W95Q64 flash memory and STM32F429 custom board. I want to load Touhgfx files to external flash memory. For this purpose, firstly I added below declarations into FLASH.id file as;

SPIFLASH (r) : ORIGIN = 0x9000000, LENGTH = 8M

and

ExtFlashSection :
 {
 *(ExtFlashSection ExtFlashSection.*)
 *(.gnu.linkonce.r.*)
 . = ALIGN(0x4);
 } >SPIFLASH
 
 FontFlashSection :
 {
 *(FontFlashSection FontFlashSection.*)
 *(.gnu.linkonce.r.*)
 . = ALIGN(0x4);
 } >SPIFLASH
 
 TextFlashSection :
 {
 *(TextFlashSection TextFlashSection.*)
 *(.gnu.linkonce.r.*)
 . = ALIGN(0x4);
 } >SPIFLASH

after compilation in CubeIde, the memory is created as shown below;

0693W000006Eu2GQAS.pngMy problem is that I dont know how to download all those files to my board. As far as I know, I need to use external loader in debugger section but there is no convenient option in the tab which is exactly match with my configuration.

0693W000006Eu67QAC.pngit will be appreciated if someone explain what to do additionally and explain all procedures step by step.

Note: I include the library and called W25qxx_Init() in the main block. The connection pins; CS -> PG3; CLK -> PB3; MOSI -> PB5; MISO -> PB4;

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
Dec 7, 2020 6:10 PM UTC

You'd have to write an external loader suitable for your part and board wiring choices. Not really a paint-by-numbers process.

If you've already coded something to initialize, erase, read and write the memory, you could integrate that into your application, allowing you to detect that the SPI isn't filled, and provide a method to download binary content via UART using say X-MODEM or Y-MODEM type protocol.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Btovi.1
Btovi.1Author
Associate
Dec 7, 2020 8:33 PM UTC

Thank you so much for the guidance ...

But it is a bad news for me :) I need to see a couple of similar examples in order to do it by myself.

Ok at least I now know what to search :)

if any ST member reads here :

Please add a video to demonstrate how to create communication between touchgfx and external memories (including sd card) as a coming part of this video. Coz you know internal memories are quite limited and not enough for developing larger projects although touchgfx is really very powerful tool for that purpose. I know it is not easy to write an interface to communicate with a not addressable thing in order to automatize that procedure but please illustrate us how to do it manually. Yes I read explanations in your website but an application example will be more helpful if you can. Thanks..

Tesla DeLorean
Guru
Dec 7, 2020 10:00 PM UTC

Do you have a data sheet for this "W95Q64" memory?

Do you currently have a viable driver, you will need something working/tested before proceeding to an external loader

This is attached to a SPI bus, it won't be mapped into the STM32's address space.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Btovi.1
Btovi.1Author
Associate
Dec 8, 2020 11:31 AM UTC

is this a good example for this aim?

Explorer
Oct 4, 2024 5:31 AM UTC

Hi Btovi.1 I had the same problem, did you solve it? If so, can you help me please?

Tesla DeLorean
Guru
Oct 4, 2024 8:19 AM UTC

This thread is from nearly 4 years ago.

Open a new question with your details.

A QSPI External Loader is not exactly suitable.of an F4 SPI implementation. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..