Skip to main content
jguo.2
Associate
Apr 5, 2022 9:28 AM UTC
Question

How to Load a binary font from a file-system to SDRAM in TouchGFX

When I malloc the fontdata[2048] in internal RAM, it work well. But when I malloc fontdata[2048] in external RAM, it go into HardFault. The external RAM is SDRAM ( W9825G6KH 32MB ).

This is the code:

#include <gui/common/FrontendApplication.hpp>

#include <fonts/GeneratedFont.hpp>

#include <texts/TypedTextDatabase.hpp>

#include <stdio.h>

uint8_t fontdata[2048] __attribute__((section(".ARM.__at_0xC14B0000")));

//binary font object using the data

BinaryFont bf;

FrontendApplication::FrontendApplication(Model& m, FrontendHeap& heap)

  : FrontendApplicationBase(m, heap)

{

LoadFontFile("1:/Font/Font_simkai_40_4bpp.bin", Typography::LARGE);

}

void FrontendApplication::LoadFontFile(const char* fileName, const touchgfx::FontId type)

{

//read the binary font from a file

FILE* font = fopen(fileName, "rb");

if (font)

{

//read data from the file

fread(fontdata, 1, 2048, font);

fclose(font);

//initialize BinaryFont object in bf using placement new

new (&bf) BinaryFont((const struct touchgfx::BinaryFontData*)fontdata);

//replace application font 'DEFAULT' with the binary font

TypedTextDatabase::setFont(type, &bf); //Font_simkai_20_4bpp

}

}

This topic has been closed for replies.