Skip to main content
MSale.1
Senior
Jun 10, 2020 1:48 PM UTC
Solved

How to limit the transfer speed from the internal ram to the display when using touchgfx but without reducing the AXI bus frequency? The controller is STM32H743

..

This topic has been closed for replies.
waclawek.jan
waclawek.janBest answer
Super User
Jun 10, 2020 2:27 PM UTC

You mean, reducing the pixel clock? It's ltdc_ker_ck, and that is the R output of PLL3 see RCC chapter.

So you have to change the R output of PLL3.

JW

7 replies

waclawek.jan
waclawek.janBest answer
Super User
Jun 10, 2020 2:27 PM UTC

You mean, reducing the pixel clock? It's ltdc_ker_ck, and that is the R output of PLL3 see RCC chapter.

So you have to change the R output of PLL3.

JW

MSale.1
MSale.1Author
Senior
Jun 10, 2020 5:26 PM UTC

@Community member​ 

Thnx

MSale.1
MSale.1Author
Senior
Jun 10, 2020 2:29 PM UTC

No not the pixel clock. i mean the speed of the bus it self for example in stm32h743 its 240Mhz at max frequency. i need to reduce it without affect the AHB2 bus

Tesla DeLorean
Guru
Jun 10, 2020 3:34 PM UTC

Yes the pixel clock, and the clocks the LTDC is using to drive the pacing of data fetches from the memory, it is a synchronous machine, want it slower, gear things down. Play with FIFO and BURST type settings to control how much data pulls at each interaction.

Don't have the bandwidth, then you're going to have to come up with a different approach.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MSale.1
MSale.1Author
Senior
Jun 10, 2020 5:25 PM UTC

@Community member​ 

Ok Thnx!

berendi
Principal
Jun 10, 2020 2:50 PM UTC

Why? What problem would that solve?