Skip to main content
MChug.1
Explorer
Oct 28, 2022 1:59 PM UTC
Question

How to get Touchgfx framework tools for compiling on an M1 Macbook?

Hi All,

I am running a docker container on an M1 macbook to build an application that uses touchgfx.

I got everything building natively on M1 macbook, except touchgfx tools (e.g. imageconvert) as in that case I get error:

qemu-x86_64: Could not open '/lib64/ld-linux-x86-64.so.2': No such file or directory

Would it be possible to get the Touchgfx framework tools that are compatible to run natively on M1 macbooks?

Best regards,

Bilal

This topic has been closed for replies.

1 reply

Yoann KLEIN
ST Employee
Oct 31, 2022 8:10 AM UTC

Hello @MChug.1​ ,

TouchGFX is not supported on MacOS, but if you use Linux, you should be able to build everything.

What is "everything building natively" for you ?

Also, did you build everything on the MacBook or did you sent them to the Mac after compiling on a Windows PC ?

/Yoann

Yoann KLEINST Software Developer | TouchGFX