Skip to main content
Visitor II
Aug 24, 2026 7:13 AM UTC
Question

How to Get and Set Scroll Position

I want to get the scroll position of a ScrollList widget in the view, and also set the scroll position in the view.However, the `setOffset` and `getOffset` functions of `ScrollBase` are protected.How can I get and set the scroll position of a scrolllist?

3 replies

ST Technical Moderator
Sep 3, 2026 1:38 PM UTC

Hello,

you can use:

int16_t getItem(int16_t drawableIndex)
virtual void animateToItem(int16_t itemIndex, int16_t animationSteps =-1)

See ScrollList | TouchGFX Documentation

Associate
Sep 6, 2026 4:09 AM UTC

It’s different, I think he hope create a ScrollBar for ScrollList.

 

One solution is use ScrollLayout, ScrollLayout can do this. But in my case ScrollLayout to slow. if you have a few data ( < 20). It is good idea. 

 

Maybe create a class MYscrollList,  class inheritance from ScrollBase but don’t protect setOffset(), getOffset() can do this.

 

Visitor II
Sep 7, 2026 4:39 AM UTC

I’ve run into a similar issue while building a music-related website. Small UI details like controlling lists and keeping the interface responsive can make a big difference. For example, I use my site to let users quickly find and check song information, so keeping the interface simple and easy to navigate is important.