Skip to main content
Tuoman
Senior II
September 15, 2020
Solved

How to generate full font files?

I need to generate font binaries for all characters, because the device accepts external inputs which is unknown at compile time and can use any characters, including chinese and japanese.

TouchGFX seems to generate font files only for characters that I use in software at compile time? Is this correct?

How can I generate full font files? Thank you!

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
September 15, 2020

TouchGFX will generate what you tell it to. If you only use static texts, then yes, that's what you'll get. But if you define wildcard-ranges to cover the entire unicode range of your font, then you will have those glyphs as well.

For chinese and japanese you'd end up with a large number of glyphs, so here you have the option of using "binary fonts" and "font caching" if you are strained on resources. You can put a binary font on an SD-card and cache the glyphs you need for each view, for instance.

/Martin

1 reply

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
September 15, 2020

TouchGFX will generate what you tell it to. If you only use static texts, then yes, that's what you'll get. But if you define wildcard-ranges to cover the entire unicode range of your font, then you will have those glyphs as well.

For chinese and japanese you'd end up with a large number of glyphs, so here you have the option of using "binary fonts" and "font caching" if you are strained on resources. You can put a binary font on an SD-card and cache the glyphs you need for each view, for instance.

/Martin