Skip to main content
V.H
Senior
Apr 13, 2022 9:21 AM UTC
Question

How to generate a big images.bin file?

Hello all,

I used a lot of images in my project and I put them (images.bin file) into SD-Card for used.

Now I have a question:

How to generate a big images.bin file?

"In this example we will put the image data in the ExtFlashSection at address 0x24000000. You can select any address that is otherwise unused (not part of the code or data address space)."

The 4GB (0x00000000~0xFFFFFFFF) zone is include code and data space, but I need to generate a big images.bin such as 4GB size.

This topic has been closed for replies.

4 replies

KnarfB
Super User
Apr 13, 2022 12:05 PM UTC

The image file for the MCU must match the MCU+Board flash addresses and sizes. The file size is independent of the size of the SD-card you're storing it on.

hth

KnarfB

V.H
V.HAuthor
Senior
Apr 14, 2022 2:24 AM UTC

For example: (stm32h730 memory map)

[0x00000000, 0x20000000] for code

[0x20000000, 0x40000000] for ram

[0x40000000, 0x60000000] for peripherals

[0x60000000, 0x70000000] & [0x90000000, 0xA0000000] & [0xC0000000, 0xE0000000] for fmc

[0x70000000, 0x80000000] & [0x90000000, 0xA0000000] for octospi

unused space only [0xA0000000, 0xB0000000] (256MB), so I put the image data in the ExtFlashSection at address 0xA0000000. This gives me a file (images.bin) containing the image byte arrays only, then I programmed this file to SD-card for used.

If my image data is more then 256MB, Keil compilation fails. Now, my image data capacity is close to 4GB, how to generate the images.bin file?

Thank you for your attention. 

Pavel A.
Apr 14, 2022 8:07 AM UTC

> If my image data is more then 256MB, Keil compilation fails

If "image" here means pictures such as jpg, png or a filesystem image - make it

using some other tool: a C or python program for example.

Compilers are best at converting C/C++ source code to binary.

Not a suitable tool for the task.