Skip to main content
ikassma
Associate III
March 23, 2019
Question

how to External QSPI Nor Flash download Image?

  • March 23, 2019
  • 8 replies
  • 1524 views

I built a Custom Board based on the STM32F769I-Discovery Board.

The other major part is the connection Pin of the QSPI Nor Flash.

Could I most easily download the image of TouchGFX to QSPI Nor Flash?

How do I download a HEX file that contains a combination of programs and images?

This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
March 23, 2019

Typically you would create an external loader for the STLINK utilities or Keil that runs in RAM and handles the board and chip ​specifics of your design.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ikassma
ikassmaAuthor
Associate III
March 23, 2019

thanks to your answer.

when i 4 days ago i will try to st-link utility custom external loader(Compile IAR8.x) but it was not working.

I also saw a lot of your answers on the ST Forum.

Are there any special considerations to customize the external Loader?

I tried very hard to keep interrup from working and I used the example of ST CUBE Programmer.

All QSPI operations did not have problems when run on internal FLASH, and the example used the QSPI BSP from the STM32F769I-disco Board.

​

thank you​

Tesla DeLorean
Guru
March 23, 2019

You'd need to review what actually gets placed in the object. The HAL model fits poorly with loader paradigm as interrupts, callbacks and systick timeout methods are not viable. The loaders are also extremely hard to debug as the JTAG/SWD is being used for the programmer.

You would want to come at this with significant understanding of linkers and loaders, and in the case here the .ELF object format. Find the team member with the most direct experience to code the loader.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Andreas Bolsch
Lead III
March 24, 2019

If you're not tied to a specific programmer you could try openOCD with either this patch

http://openocd.zylin.com/4321

or that one

http://openocd.zylin.com/4760

The configuration according to a specific board isn't that complicated. However, you have to build openOCD with the patch yourself. On Linux that's almost trivial, on Windows it's probably not that trivial.

Note that this affects only the actual flash programming, not the whole toolchain, you can still use any compiler/linker/IDE.

ikassma
ikassmaAuthor
Associate III
March 25, 2019

thanks for your answer ^^

ikassma
ikassmaAuthor
Associate III
April 1, 2019

i solved this problems.