Skip to main content
Mk.31
Associate II
April 19, 2021
Question

How to develop a UI from touch GFX for the custom TFT displays (SPI Interface)

Hi,

I'm using a custom matrix orbital TFT display which is interfaced to the STM32H7B3-DK board through SPI. How to implement developed a UI from TouchGFX to the custom display. Referred to an FMC and SPI interface section, need better clarification. Please suggest a solution.

This topic has been closed for replies.

5 replies

Romain DIELEMAN
ST Employee
April 19, 2021

Hi,

Just to clarify the situation, you are working with an STM32H7B3-dk board and wish to change the display to your custom one ?

Have you started your project from scratch or did you use the application template for the STM32H7B3dk board available in TouchGFX Designer ? If the second scenario then you will need to modify the TouchGFX Generator in CubeMX and write a TouchGFX driver. Have a look and follow this guide on FMC and SPI Display Interface in the online documentation. Badreddine from ST also made a video on how to customize a TouchGFX template for STM32H7B3-dk boards. Even though he is not using the same display interface as you the main steps are the same. You can also have a look at the application template of the STM32G0nucleo board available in TouchGFX Designer. This board is also using a SPI display so you can look at the STM32CubeMXsettings and the code to have a better understanding of what to do.

/Romain

Mk.31
Mk.31Author
Associate II
April 20, 2021

Do we need to write a driver's code for all the DK boards with built-in display and DK boards interfacing with the custom display while generating the project from cubeMX? I tried generating code for the STM32H7B3I-DK board (for built-in display) BSP driver files not generated when I generated code from the cubeMX and while debugging it is going to hardfault.

If you generate the code from touch GFX no issues everything working fine.

Romain DIELEMAN
ST Employee
April 20, 2021

Hi,

When you create a project with an application template for an ST development board you will have a preconfigured project where we did all those steps for you. This is why you are missing the BSP files for example like you said.

/Romain