Skip to main content
D..1
Associate
Sep 2, 2020 6:57 AM UTC
Solved

How to create customized busyIndicator?

..

This topic has been closed for replies.
Romain DIELEMAN
Romain DIELEMANBest answer
ST Employee
Sep 2, 2020 11:11 AM UTC

The circleProgress widget would be a good way to do this. Have a look at the documentation and at the UI example "Progress Indicator" there are examples of progress bars/circles that could be interesting to you as they can be sued as loading process. There are some code as well to help you get started.

13 replies

Romain DIELEMAN
ST Employee
Sep 2, 2020 8:26 AM UTC

Hi friend,

Could you be a bit more specific? What do you mean by busyIndicator? What have you tried for now?

/Romain

D..1
D..1Author
Associate
Sep 2, 2020 9:03 AM UTC

I want to create a widget indicating the process is going on and to wait.

ex. a spinning wheel.

Romain DIELEMAN
ST Employee
Sep 2, 2020 10:10 AM UTC

So like a text saying "it is working now, wait" ?

KNara.2
Associate III
Jan 18, 2023 12:48 PM UTC

Thanks for pointing out the example projects in TouchGFX.

But would like to know how the busy indicator was implemented?

Is it using Circleprogress indicator or Circle(shape)?

Or is it circle in combination with text mapper?

Circle widget can be used to implement a busy indicator.

Would like to know how to make the trailing end of the circle as faded for a busy indicator.

Also how to set the circle to rotate for a specified amount of time?

Please help.