Associate
Apr 6, 2016 8:47 AM UTC
Question
How to convert DCMI captured raw RAM bufferd data into human visible image formate in PC?
- 3 replies
- 1227 views
Posted on April 06, 2016 at 10:47
Hi Folks,
I have interfaced OVM7692 CMOS camera with stm32f4xx MCU using DCMI interface.After capturing image i am taking data into RAM buffer and i have printed those data into UART console and hence i have got the hex values of those images.Now from uart I have taken them into .txt format (sample is attached here.)Now my query is after getting these data into PC how can i convert them into human visible image ?Is there any PC software available or any one have done it before ?Can I do it with python ? if so how can i proceed ?Is there any other way ?OVM7692 has RAW 8-bit, RGB565, QCIF 176x144 (60 fps) features.Please suggest me here, also let me know if i can provide any more details on the same.Any help on this would be great appreciable.Thanks & Regards,Rutvij. #pc #software #dcmi #ovm7692