Skip to main content
Jloda.11
Associate
October 22, 2021
Question

How to connect a custom LCD diaplay to touchgfx? and where to get a 7 inch LCD display?

I want to use a custom 7 inch LCD display in my project, here are my requirements and some questions.

My project requirement is:

  1. A 7 inch or more LCD display
  2. Capacitive touch
  3. 1080 x 600 or 800 x 480 Resolution

questions:

  1. From where do I get a 7-inch LCD display
  2. how do I use a custom 7 inch LCD display with touchgfx
  3. Are any discovery boards available with a 7-inch LCD display
  4. I already have an stm32f7508 discovery board can I connect it to a 7 inch LCD display

This topic has been closed for replies.

1 reply

Romain DIELEMAN
ST Employee
October 22, 2021

Hi,

There are no ST discovery board with a 7 inch display to my knowledge, but I know that the STM32H7B3 evaluation board has a 7" 800*480 TFT RGB LCD display.

To understand how to setup the display with the ST toolchain have a look at the Board Bring Up articles in the documentation . There are also a couple of videos made by ST and other users which can be of use. Depending on the display interface you will use you can have a look at the relevant TouchGFX Board Setups and Board Specific Demos available in TouchGFX Designer and use them as source of inspiration for your configuration.

It is a bit difficult to say if an STM32F7508 discovery board will be able to use a 7 inch display, I can just point that the framebuffer necessary for a 1080*600 resolution will be HUGE so watch out for the memory consumption. Otherwise stick to a 800*480 with 16bpp ( framebuffer size = Width * Height * bpp/8 = 768 000, so still huge).

Now, where you can get a 7-inch display ? Well that kind of depends where you are located and the amount of display you want. I'll let other users comment on this.

/Romain