Skip to main content
PM.5
Associate III
Jul 29, 2022 9:58 AM UTC
Question

How to configure graphical display in bare metal ?

Hi,

I am working on stm32f746g -disco board. I tried it with TOUCHGFX it worked ,but it is on FREERTOS. I tried by disabling FREERTOS & again regenerating code through TOUCHGFX ,it is executing with OSwrappers file which is an adapter between OS and driver. I want to operate the graphical display in bare metal , so that I can understand the code & make the changes as per my requirement. If anyone have an idea on that please let me know.

Thanks.

This topic has been closed for replies.

9 replies

Tesla DeLorean
Guru
Jul 29, 2022 12:21 PM UTC

What does that mean, without the RTOS, or at a register configuration level.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PM.5
PM.5Author
Associate III
Jul 29, 2022 12:26 PM UTC

without the RTOS

MM..1
Super User
Jul 29, 2022 2:31 PM UTC

What is your question? Error? Why yuo dont understand code with or without OS?

PM.5
PM.5Author
Associate III
Jul 30, 2022 3:56 AM UTC

I understand the code of RTOS , but my requirement is to do on bare metal(without RTOS ).

MM..1
Super User
Jul 30, 2022 9:51 AM UTC

In MX wizard untick RTOS in touchgfx and addware config , delete manualy target folder in Touchgfx , after this close MX and generate bare metal code. Or create new project .

Switching methods in existed project dont work ok.