Skip to main content
SNC.1
Associate II
Mar 31, 2023 4:08 AM UTC
Question

how to change the animation in stm32f7?

i have tried by using touchGFX, when i press the "target run" it's showing failed, but when i do "Run simulator", There is no error in it.

This topic has been closed for replies.

4 replies

Yoann KLEIN
ST Employee
Mar 31, 2023 8:10 AM UTC

Hello @SNC.1​,

Could you provide more information about the error message ?

Did you start your project with a TouchGFX Board Setup (from TouchGFXDesigner), or from STM32CubeMX ?

Did you ensure that your board is correctly connected and powered ?

/Yoann

Yoann KLEINST Software Developer | TouchGFX
SNC.1
SNC.1Author
Associate II
Apr 3, 2023 3:52 AM UTC

i started my project with TouchGFXDesigner.

Yoann KLEIN
ST Employee
Apr 24, 2023 11:20 AM UTC

Sorry for the delay,

Are you sure the board is correctly connected and powered ?

/Yoann

Yoann KLEINST Software Developer | TouchGFX
Osman SOYKURT
ST Technical Moderator
Apr 24, 2023 11:43 AM UTC

Hello @SNC.1,

Do you have STM32CubeProgrammer Software installed on your computer? Running on target with TouchGFX Designer requires STM32CubeProgrammer software so if you don't have it, you'll need to install it.

/Osman

ST Software Developer | TouchGFX